Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Follow the steps listed below to send a CAD model to your e-mail address.
Make sure that you are in the dialog area 3D CAD CATALOGS and navigate to the required part.
In the dialog area Download CAD models under Edit CAD formats -> Add CAD formats, select the transfer mode email by clicking into the option field. Then define one or more CAD formats and confirm your entries by clicking on Save.
-> The view returns to the dialog area Generation options / Selected formats. Confirm your entries by clicking on Save.
Under Actions, click on Generate CAD MODEL.
Note
All formats selected under Download CAD models (dialog area 3D CAD CATALOGS) -> Edit CAD formats ->Selected Formats are generated.
As long as the generation is running, is shown.
As soon as the generation has completed, you will get informed by the note Check your emails that the component was sent by e-mail.
If you close this window, further CAD models can be selected.
Furthermore all generated CAD models are listed under Download CAD models.
After clicking on the link Info specific part information is displayed:
Status information about generation
All formats activated under Download CAD models (dialog area 3D CAD CATALOGS) -> Edit CAD formats -> Selected formats are generated and listed here now.
For some formats you can get some CAD specific information by clicking the Info-Icon .
The same Info icon you can find underDownload CAD models -> Actions.
In order to import models into the CAD system, do the following: