Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the following you can see how to classify a conveyor belt and to test the simulation in the Mechatronics Concept Designer.
Note | |
---|---|
Precondition is a current CNS classification. Install it in PARTadmin under Catalog update -> Online -> selection Classifications.
|
In the Configurator, select the part to be classified in the assembly (the belt in the conveyor belt) and open it via context menu command in PARTproject.
Under Project selection, select the 3db file.
-> On the right under Edit project, a Preview is displayed (here in the example in hand the belt).
On the feature to be classified (here a face), call the context menu command Face.
In the case of a conveyor belt select the class under Simulation -> Assembly Line.
-> Beside the selected class the single Features are displayed.
In the case of a conveyor belt please set the following values:
Direction: Direction vector for conveying. It has to be parallel to the face of the conveyor belt. Set X to 1 and Y and Z to 0.
Scroll down to see the parameters at the end of the list.
Values for 3D identification and 3D Filename are automatically set. Metadata may be empty.
Export the conveyor belt to NX by clicking on .
In NX under Application -> More, open the Mechatronics Concept Designer.
-> Under Sensors and Actuators you can see the classified transport face.
In the context menu, click on Edit.
-> The dialog box Transport Surface is opened.
As you can see, Vector, Velocity and Name have been transferred from the classification.
In addition, place a test object on the conveyor belt and start the simulation by clicking on the “Start” button .