Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
-> The sketch is opened in the 3D view.
-> The command Extrude... opens the dialog box Extrusion solid.
Once all entries are made a preview is displayed in the 3D view. Changes are immediately displayed.
Name: Per default "Base extrude <number>" shows up. The numbers go up consecutively with each new extrusion.
In the Length field you can set the measurement of the stretch of the 2D object.
Opposite direction: The extrusion is performed in opposite direction. |
Both directions: The extrusion is performed in both directions. |
|
|
Draft: In order to create a draft from a 2D sketch, enter the respective angle measurements into the draft field. |
You can connect a Condition to an extrusion as well. Possible characters are &, |, !=, =, >, <, >= and <=. |
Example: The sketch should only be extruded if for variable H (height) a value larger than 10 has been set. |
Construction steps (features) which, based on their condition are excluded, will be deactivated in the 3D History and identified by an if symbol ( at Base at Cut) .
In some rare situations we have the problem that we need to increase the accuracy for rasterization within the part to enable the creation of certain geometry. Therefore you can find this option for Base, Cut and Sweep.