Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Basic settings for the lighting situation
Per default a file is already set up. Via Browse you may change the file. The Maxwell installation brings some sample files with it, which you may select here.
A default value is already assigned. Adjust the value if you like.
The stage on which the part is located, is already set up per default.
In the list field select the desired option:
A *.mxs file is created without starting either the Renderer or the Studio. The file can later be opened in the Renderer or in the Studio.
Start renderer: Select this setting in order to create an image file.
When there is a server installation which you can access, select Transfer to server.
Then during the export the PARTrenderManager dialog box opens.
Via the PARTrenderManager you get additional options for rendering. A detailed description on this can be found under Section 3.1.9.3.3.6, “PARTrenderManager with Maxwell Renderer ”.
Quit after rendering: Closes the Renderer after the image file was created
Stop renderer after: Setting for the sample run-through (editing steps)
The more editing steps are carried out, the more accurate will the details be displayed.
Here you can determine the sampling rate. If no sampling rate is entered, the value is automatically set on 10.
If you do not want to edit the MXS file later in the Renderer or Studio you can delete it.
This file saves the render status up to date, so that you can later carry out more sample run-throughs.
The following image formats are available for use in the selection listg: bmp, tga, jpg, png, png (transparent), tif, jp2, exr, ppm, pbm, pgm, hdr
If you do not activate the checkbox, then you may define the rotation with your own values.
If you do not activate the checkbox, you cannot define your own values under Resolution.
Threads: No threads, Only outer threads, Only inner threads, Only visible threads, All threads