The menu item
PARTserver/PARTcommunity is displayed at
directory and project level.
Additional files:
Visible at
directory level.
Enter those
files here that should be copied after PARTserver/PARTcommuntiy. Per
default the add-on ",0" is added.
Should an
entire subdirectory need to be copied (for ex., needed for assistants)
however, then specify the subdirectory and change the parameter to
"1".