Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.10.7.
Optional parameters Details
5.10.7.1. Correct display
of inch variables in dimensionings
|
|
---|---|
Prev | Next |
As of V11 SP9 decimal values in dimensionings can be displayed as fraction.
For this use following expression:
%frac%[accuracy]
"{0.75%frac%2}" is displayed as "3/4".
Mixed text for dimensionings is also possible:
"{0.75%frac%2} = {0.75}" is displayed as "3/4 = 0.75".
Important | |
---|---|
The accuracy of values determines how many decimal places will be considered. So "{0.75%frac%1}" is displayed as "4/5", because 0.75 is rounded to 1 decimal place (0.8 -> 4/5). |
Maximum value for accuracy is 9. Higher values are set back to 9 internally.
If a part is opened in a version that does not support fractions, the decimal value will show up.