Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.13.10.15. Classify
Electrical Parts - Tutorial
5.13.10.15.6. Class
"Electrical Connection" (CNS_CP|4|3) -> Attribute "Connection Name
Equivalences"
|
|
---|---|
Prev | Next |
The field Connection Name Equivalences is used in order to designate which connection points (if any) have the same electrical potential, meaning those connection points that have a physical (conductive) electrical connection to the connection point you are currently classifying.
In the CNS classification this is done under class CNS_CP|4|3 (Electrical Connection) with the attributes Identifier and Connection Name Equivalences.
From the electrical diagram above, we see which connection points have the same potential:
Connection Name Equivalences | S2
Connection Name Equivalences | S1
In the case that there are more connection points with the same potential, for example S1, S2, S3, S4, it would look like this:
Connection Name Equivalences | S2||S3||S4
Connection Name Equivalences | S1||S3||S4
Connection Name Equivalences | S1||S2||S4
Connection Name Equivalences | S1||S2||S3