Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
3.2.18. Classification
according to CNSORDERNO / CNSTYPECODE
3.2.18.3. Plugin
"Resolve check"
|
|
---|---|
Prev | Next |
Use case and Rahmenbedingungen:
In order for parts to be found via search for Order number or Type code, included those where CNSORDERNO and CNSTYPECODE are build by value range values, certain preconditions have to be fulfilled. If the number of possible combinations resulting from the value ranges is too big, no indexing will take place, but instead a Reverse Search is used, which enables finding of value range values as well.
The Resolve check checks if a catalog is resolvable in the full-text search index or if a Reverse Search is necessary. If the catalog is accordingly prepared, even in most complex cases searching for Order number or Type code will be successful.
The Resolve check shows which measures need to be taken in order for all projects and rows to be found.
Right-click on a catalog or directory -> Automation -> Resolve check
The initial check may last a bit depending on catalog size.
The result of the analysis is displayed in a dialog box.
When clicking on Apply the respective settings are automatically performed.
Details on this can be found under Section 5.8.2.1.15.18, “Reverse search ‒ Resolve check (automatic) ”.