Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The required
JSPs have to be stored in the customer's Windchill system. For this,
normally they are stored by the customer in a subfolder of the directory
<WindchillInstallDirectory>\Windchill\codebase\infoengine\jsp
.
Then for each
JSP the URL used for calling the respective JSP has to be stored in the
configuration file <windchill_public_api.cfg>,
in
the section [JspPaths]
. Normally the URL
has the following format.
http://<WindchillServer>/Windchill/infoengine/jsp/<Unterverzeichnisstruktur>/<JSPDateiname>
Should the JSPs be stored at another place by customer, the URL has to be provided by the customer.
Not always all JSPs are needed (see description of the respective JSP).
In order to be
able to access the JSPs, login data (user, password) is required.
Depending on the use they can be stored in the configuration files
ifproepdmlink.cfg
or
pdmProxies.cfg
.
Required for the function AddLinkedWTPartToWorkspace.
Get the Workspace identified by <workspaceName>, get the EPMDcoument identified by <documentSearchAttribute><documentSearchValue> from the workspace, get the linked WTPart(s) from the EPMDocument and add it/them to the Workspace.
Required for the function ChangeIdentity.
Searches for a Windchill object and sets the attribute <attrToChange> to <newVal>.
Required for the function CreateAndLinkPart.
Search for document by <epmDocSearchKey>==<epmDocSearchValue>. IF no document is found execution is aborted with an appropriate error message!
IF <wtPartSearchKey> & <wtPartSearchValue> are set: Search for a part of type <partType> using these values.
IF no part is found in (2) & <createPart> is set to 1: Create new part (if attribute "name" is not provided the name of the EPMDocument will be used the same applies to "number")
IF no part is found in (2) & <createPart> is set to 0: Execution is aborted with an appropriate error message!
Required for the NativeCheckin.
Searches for CAD document and returns 1 if it exists and 0 if not.
Required for the function searchDocumentByAttributes.
type | |
ReturnAttribute | The name of the document attribute to use for the returned list. Default is "CADname". |
WHERE_CLAUSE | The WHERE clause to use for the search. |
Performs the search and returns a "|" separated list of document names containing the name of each document that matches all search criteria.
Required for the document search of PdmProxies (PLMSynchro query).
Get folder, library, product or context OIDs.
Required for the data query of PdmProxies (PLMSynchro data retrieval).
For each ObjectIdentifier the EPMDcoument is retrieved and it's data is written to the returned XML. Gets data from EPMDocument and Element objects. Optionally retrieves components / family table member data.
Required for the document download of PdmProxies (PLMSynchro download).
Searches for a Windchill object and returns a download link.
Required for the function GetObjectAttribute.
Searches for a Windchill object using <type>, <searchKey>, <searchValue> and returns the value of the attribute given by <attributeName>.
Always required once JSPs are used. Used for the testing of connection.
Required for the functions MoveObjects, MoveObject and Move part.
Move Windchill object(s) given by <searchKey>=<searchValue> to folder given by <library> & <path>.
Required for the document search of PdmProxies (PLMSynchro query).
Search for Windchill documents using the Search-Objects webject.
Always required once JSPs are used. Used for the error management of the other JSPs.