Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Altreps is supported as of NX 10.
In order to support native placing of "alternative representations" for NX10, the macro "cns_place_nx10_teamcenter_altrep.macro" has to be used. In addition to already available placeholders two new have been added: <<CNS_ITEMREVINDEX>> and <<CNS_ALTREPINDEX>>. These have to replace the numbers in the following macro lines when self-recording:
CUSTOM 25 PdmUI_BrowseApp * TL_EXPAND * (1) * 1 ! CUSTOM 25 PdmUI_BrowseApp * TL_EXPAND * (1 <<CNS_ITEMREVINDEX>>) * 1 ! CUSTOM 25 PdmUI_BrowseApp * TL_PICKED_ITEM * (1 <<CNS_ITEMREVINDEX>> <<CNS_ALTREPINDEX>>) * 0 ! CUSTOM 25 PdmUI_BrowseApp * TL_SELECT * (1) * 0 * 0 ! ... CUSTOM 25 PdmUI_BrowseApp * TL_SELECT * (1 <<CNS_ITEMREVINDEX>> <<CNS_ALTREPINDEX>>) * 0 * 1 !
NX 11 and 12 do not need the special macro. The "normal" placing macros are sufficient.
In addition, in ifnxteamcenter.cfg, the key TC_allowItemAltRep=1 has to be set for customers, which have activated Altreps for templates (<ShowAltrep>Yes</ShowAltrep> in the respective .pax file). This applies for all versions.