Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following example shows the settings for manual database login at PARTdataManager start and direct client database connection (= using the options Catalog browsing and search with AppServer or Search with AppServer ).
When using the setting option Catalog browsing and search with AppServer or Search with AppServer the connection between client and link database is directly established. Meaning ODBC has to be set up on the client.
The name used for setting up the ODBC connection has to be identic with the entry under PARTlinkManager -> Extras menu -> Configure ERP environment -> tabbed page Database -> Name.
Set environment variable CADENAS_DATA on the client
The environment variable $CADENAS_DATA has to be set and point to the data directory (on the server).
Note | |
---|---|
In contrary, this is not necessary when the option Catalog browsing, search and database with AppServer is used because then the connection to $CADENAS_DATA is established via AppServer. |
The following settings have to be made on the AppServer:
PARTadmin -> category ERP environment -> Database login -> Enable automatic login
If a login dialog for user authentication shall be displayed at PARTdataManager start, please make sure that the option Enable automatic login is disabled.
Change to the category ERP environment -> User.
Under User-Role assignment on the left side under User, click on and create the required PARTsolutions users (here exemplified the users "ecat" and "location") and on the right side, enable the desired roles which shall be available to the respective user.
Create the same users in the database.
|
The input fields under Login-Dialog and Automatic login can remain empty because the authentication data is entered in the login dialog at PARTdataManager start and is checked directly at the database.
Result: At PARTdataManager start the Database login dialog opens.