Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
When generating
the CIP file of a catalog, in the catalog's filedir.prj
the results of the
resolve check will be set in the form of following keys (for details see
Section 5.8.2.1.15.18, “Reverse search ‒
Resolve check (automatic) ” in eCATALOGsolutions Manual):
CATMETRICS_SEARCHABLE_PROJECTS
Number of projects which should be found (All visible projects and projects with SEARCHINDEX=ON)
Number of projects with a classified order number or type code variable
Number of projects with order numbers and type codes indexed by lucene
Number of projects which can be solved via auto reverse search
Number of projects which can't be found by the reverse search
Background
information: In order to create the information which shall be written
into the dir.prj
, the
configuration files resolvecheck.cfg
and *.qacheck
are evaluated. E.g., the
ResolveChecker writes
to resolvecheck.cfg
for which projects an automatic Reverse Search is possible. For the case
that someone changed a project without executing the ResolveChecker the information
is read from *.qacheck
, where Testmeta is writing
to, and for changed projects Testmeta has to be called in any case,
because otherwise publication is not possible.