Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the Details mode you will receive more information such as Name, Description, Version, Unit, End date, etc. in a table view.
To navigate in the depths, double-click on a row.
Results after double-clicking:
The selected directory shows up in the breadcrumbs row. (See Section 3.1.6.4.12.7, “ Navigation via navigation path (breadcrumbs) ”)
On the right, in the Part selection, now elements of the next deeper level are displayed.
Navigate by clicking on desired directories or elements in the breadcrumbs line (see Section 3.1.6.4.12.7, “ Navigation via navigation path (breadcrumbs) ”).
On the left in the tree, the respective level is also selected.
Especially when a small preview image is shown, it is helpful to display 3D Tooltip + Technical details (if available). Hereto move the mouse over the preview image.
The 3D Tooltip is scalable and animated. In the down right corner you can find a drag point to draw up the size. The extensions of X, Y and Z axis are automatically displayed.
In PARTdataManager under Extras menu -> Preferences... -> Part selection, you can determine, whether and how the tooltip shall be displayed..
Via clicking on a column header, you can sort the rows depending on the values of the desired column.
If you use ERP integration, then you can sort via the red-green folder characteristic in addition.