Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Some parts have Value range variables. For these no fixed value is specified.
In the vertical view these parts are marked by :
|
In order to specify the concrete characteristic, all value ranges have to be specified as well.
Depending on part specifications there are different ways of value range selection.
When changing a value the depiction in 3D view is immediately adjusted.
Value range: Enter the desired value within the value range or choose the value via slider.
The red line marks the default value. When clicking on it the default value is set again.
Selection of discrete values: In the list field, select the desired option.
Selection of discrete values with preview images:
To clarify the selection options in value range fields, graphics can also be displayed. Select the desired option via double-click.
Meaning of colors in value range fields
Note | |
---|---|
Colors have to be activated. See above. |
Depending on pre-settings, colors are displayed in the symbol , which point out different types of value range fields.
The Function attribute is used for stroke and angularity, everything which defines a mechanical movement in a part / assembly (e.g. the rod positioning of a cylinder). |
Dark yellow = Dimension attribute
The Dimension attribute is used for half-finished products and profiles that do not have fixed dimensions. |