Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
On the General tabbed page you have the following setting options available:
Maximum number of search results : Set the desired value.
With each click on the next block of results is displayed successively.
Show suppressed option dialogs again:
Example on Geometric search (3D) is also valid for LIVEsearch -> Automatically update best result in part compare.
In the dialog box Geometric search (3D), click on Load file.
Select the desired file and confirm with .
-> The dialog box Selection of file format is opened.
Determine the desired format and confirm with .
-> The respective dialog box for Import options is opened.
Open dialog for search options when searching via context menu:
This option concerns the dialog box Geometric search (3D).
The option is deactivated by default, because in this case no search part has to be selected.
However, if settings shall be performed, activate the option.
If this option is activated the dialog box appears, otherwise the search is directly performed with the options set in the window.
Use table settings for ERP columns:
When clicking the secondary mouse key in any column header, the dialog box Select columns can be opened.
When activating ERP variables here, then these are displayed in the table of search results.
If the layout settings such as color of columns or text (as displayed in the Part view by default) shall also be displayed under Search results (mode Details and Table), activate the option Use table settings for ERP columns.[121]
[121] Colors of columns and values (possibly depending on value), etc. can be set by administration. See Section 4.8, “Table layout for PARTdataManager and (PARTlinkManager) ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.