Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following explains how to create Media Variables in PARTproject. Alternatively they could also be created PARTtemplateDesigner (see Chapter 10, PARTtemplateDesigner - Create datasheets ).
Under Project selection, select the project for which you want to create Media Variables.
Under Edit project, select the tabbed page Documents.
The working area has a lot of functions from which however, only a small part is needed.
Some important points, which will help to get you started:
On the right side, you can find the filter areas Key, Language, Template and Role, which can be opened or closed.
When clicking on the icon Choose nothing you can be sure that no filters are accidentally set.
The dialog area Derivation hierarchy is only needed if contents have been created for a special project, however, then shall be made available for all projects, for example.
Open the dialog box Properties (Text view / HTML view) by clicking on .
When confirming with the displayed content is applied to the selected key and the dialog box is closed.
At first create the default language. That's why you have to select "default" under language. (Languages without content are shown grayed out.)
In the dialog area Key, click on the icon New Entry .
When clicking on , the dialog box Insert entry is opened (as in each further case when creating a new Media Variable).
In the input field, enter the name of the Media Variable to be created.
If you create variables for additional tooltip information in PARTcommunity (compare Fig. „Tooltip with additional information on PARTcommunity:“), please use the following Schema:
Variablename_HELP
For a variable BNEB, you want to create a HELP variable: Then the name has to be BNEB_HELP.
In the list field, choose the option HTMLTEXT.
Only the option HTMLTEXT, may be DIR in addition, are needed for the creation of Media Variables.
Translation: If translations shall be performed via tabbed page Translation in the course of the whole catalog translation, in any case activate the checkbox. Alternatively you could translate Media Variables on the tabbed page Documents only.
Publish: The checkbox should always be activated. Only deactivate for internal content which shall be excluded from generation.
Sort: This option should only be displayed if DIR is selected in the list field.
With the help of DIR you can create directories which can be used for sorting by moving Media Variables into them. For publishing sorting is not relevant. It only serves for a better overview.
-> In the first step, the new key is displayed grayed out. Only after assigning content, the key will be activated (and displayed in black color).
Numerical values behind the keys show how often the variable occurs (total number over all projects, languages, roles, etc.).
-> The dialog box Properties with the tabbed page Text view is opened.
On the tabbed page Text view or HTML view, enter the desired content.
<html><head><meta name="qrichtext" content="1" /><style type="text/css"> p, li { white-space: pre-wrap; } </style></head><body style=" font-family:'Tahoma'; font-size:12pt;"> <div> p, li { white-space: pre-wrap; } </style></head><body style=" font-family:'Tahoma'; font-size:12pt;"> <div> <p>The conveying direction determines the belt inlet (start) and the belt outlet... ... ...</p> <p><strong>Note</strong></p><p> ... ...</p> <p><img src="bandbreiten.png" width="100%" height="auto" /></p> </div> </html>
|
-> The content is taken into the key.
If the content shall be used on PARTcommunity as additional tooltip information (HELP information), please set the following entry in the project file:
INFO(BNEL)=BNEL_HELP INFO(BNEB)=BNEB_HELP etc.
Through this, the icon calling the tooltip information is created.
Example for additional tooltip information on PARTcommunity: