Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
You can colour a blend via PARTproject -> Show project -> tabbed page General -> Color and texture -> Color. However, in this way the whole part is colored.
|
Preference face selection over edge selection
If edge selection and face selection lead to the same result, in complex cases, basically, use face selection. If only one or two certain edges shall be edited for example, you can decide for the more comfortable and quicker proceeding.
When taking this into account, there will be created less features in CAD systems and there won´t be problems with parametric parts!
Details on face selection can be found under Section 7.9.3.10.1.5.5, “Face selection”.
For a better performance you can deactivate the Preview presentation. Details can be found under Section 7.9.3.10.1.5.4, “ Preview presentation for Chamfer/Fillet ”.
For a STEP-Export, generally, only STEP should be used, NO STEP 3D, as this format does not support the blend feature.
In version 11.00 SP3 there are some graphical glitches. They only occur in the PARTsolutions 3D view. When exporting the part, it is correctly transferred.
Sometimes the glitch can be avoided by choosing another method for the creation of chamfer or fillet.
If edges do not meet, create the blend as two different blends instead of one “big” blend.
In rare cases it is possible that symmetric parts show a defect due to a certain sequence of blend selection.[95]Changing the sequence of selected blends should solve the problem.
In SP3 there is a glitch in the 3D preview when using the Blend feature for a tapered body. The glitch only occurs in the PARTsolutions preview, so that PARTsolutions 2D derivation and exported part will be correctly.[96] There are still some more graphical glitches, but they all should only concern the PARTsolutions 3D view, so that the PARTsolutions 2D derivation and the exported part will be correctly.