Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order to post-install or remove different program features, open the installation routine.
Program features can be among others:[11]
Program packages such as PARTsolutions, eCATALOGsolutions or PARTstatistic
CAD interfaces
EDM/PDM/PLM interfaces
Catalogs
Classifications
Do the following:
Insert the DVD.
--> The start screen shows up.
(Should autostart be deactivated, double-click on "start.exe" in the Windows Explorer.)
Select the country.
Start the desired type of installation:
Installation (single workstation/Client) and/or
Installation (Server)
Close the startup screen.
The installation routine begins.
--> The dialog at the right shows up.
Select Add/remove single program features.
Follow the instructions of the installation.
Change or remove program
[11] Also see Section 3.1.1, “Installation of Software ”.