Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In this config the structure of toolbars and menus is specified.
Note | |
---|---|
Normally you don't have to change these settings. Visibility of elements is controlled by menuvisibility_PARTproject.cfg. |
For general explanations please see menustructure_PARTdataManager.cfg.
[Tweakmenu] toolbarOrderTop=Standard,LinkDatabase toolbarOrderRight= toolbarOrderLeft= toolbarOrderBottom=
Compare menustructure_PARTdataManager.cfg.
If you want to explicitly adjust the layout of the buttons, then set the value of “<name>ToolbarButtonStyle”. Compare menustructure_PARTdataManager.cfg.
The values of the key menuOrder represent the desired sequence of the single menus.
Menu name | Action name |
File | FileMenu |
Versioning system | QAMenu |
ERP | ErpMenu |
Extras | ExtrasMenu |
Window | WindowMenu |
Help | HelpMenu |
menuOrder=FileMenu,QAMenu,ErpMenu,ExtrasMenu,WindowMenu,HelpMenu
Normally the key values don't have to be changed.
FileMenuName=FileMenu FileMenuTitle=&File FileMenuContent=FileSave,FileSaveAll,-,FileExportTrans,FileImportTrans,-, actionRecentFilesList,-,FileExit
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
Normally the key values don't have to be changed.
QAMenuName=QAMenu QAMenuTitle=&Versionsverwaltung QAMenuContent=QALogin,QALegend
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
Normally the key values don't have to be changed.
ErpMenuName=ErpMenu ErpMenuTitle=ERP ErpMenuContent=LinkDbLogin,LinkDbChangeGroup,CallLinkMgr,LinkDbShowLegend,PreferredRanges
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
Normally the key values don't have to be changed.
ExtrasMenuName=ExtrasMenu ExtrasMenuTitle=E&xtras ExtrasMenuContent=ExtrasOfflineCD,ExtrasCipCatalog,-,actionPluginList,-, ExtrasEditClassSystem,ExtrasExportCSystemTranslation,ExtrasImportCSystemTranslation,-, ExtrasMessageList,-,ModePreferences,-,ShowPreferences
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
Normally the key values don't have to be changed.
WindowMenuName=WindowMenu WindowMenuTitle=&Window WindowMenuContent=actionWindowCascade,WindowsTile,WindowsTree,WindowsEdit,WindowsPreview
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
Normally the key values don't have to be changed.
HelpMenuName=HelpMenu HelpMenuTitle=&? HelpMenuContent=HelpHelp,HelpAbout,-,HelpLicenses,HelpSysInfo
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
Normally the key values don't have to be changed.
StandardToolbar=MainWindow/Standard StandardToolbarTitle=Standard StandardToolbarContent=FileSearch,-,FileSave,FileSaveAll,-,UpdateIndex,ShowPublishingState
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
Normally the key values don't have to be changed.
LinkDatabaseToolbar=MainWindow/LinkDatabase LinkDataBaseToolbarTitle=Link database LinkDatabaseToolbarContent=LinkDbLogin,LinkDbChangeGroup,CallLinkMgr,LinkDbShowLegend, PreferredRanges
Individual adjustments happen in the configuration file menuvisibility_PARTProject.cfg.
In the block [hasSubMenuActions], all actions with an additional menu level are stored. The name of top level actions is set as key. The lower level actions are listed comma separated in the line.
[hasSubMenuActions] listOfMenus=actionRecentFilesList actionRecentFilesListName= RecentFile_Menu2Content=RecentFile_Menu0_Entry6,RecentFile_Menu0_Entry7, RecentFile_Menu0_Entry8,RecentFile_Menu0_Entry9,RecentFile_Menu0_Entry10