Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the
following the structure of the AttributeMapping(is3d) if<cadname>.cfg
block is
described.
The block AttributeMapping(is3d) contains sections (here a group of keys is meant). The single sections are incremented with 00[53],01, 02, etc.
Attr_Content (optional; "Attr_Content" or "Attr_CopyFrom" must be declared, or both)
The key value refers to a same-named block in the configuration file.[54]
In the added block (tab page) "CadDocumentAttributes" custom or CAD-specific attributes can be declared.
If the value is not set the content can be specified by „CopyFrom“. If both ("CopyFrom" and "Content") is specified the content of both is merged in form of a list.
Attr_CopyFrom (optional; "Attr_Content" or "Attr_CopyFrom" must be given)
If the key exists and contains a value then this means that the PARTsolutions default attributes are transferred to the CAD system.
The following values are possible:
default: The attributes are transferred in the $CADENAS_LANGUAGE.
set language (german, english, french, etc.): The default attributes are transferred in the set language.
Note | |
---|---|
If in the set language there is no translation available in the given language then no attribute is transferred (nor the one from $CADENAS_LANGUAGE language). |
No entry: No default attributes will be transferred. (In order to transfer certain attributes, please see the information in the following chapters.
A system key (the target [e.g. tabbed page] in the CAD), which must not be modified.
A prefix can be used (e.g. CNS_). If several languages are transferred then using prefixes for differentiation makes sense in any case.
Note | |
---|---|
The structure of other tab pages is described specifically for each CAD system. Click on the desired link to jump in the CAD specific chapter. |